Other Parts Discussed in Thread: AWR1843,
Tool/software: Code Composer Studio
Hi,
Now we want to use beamforming technique on AWR1843 EVM.I have some doubts about beamforming technique.
The first question is which direction is the steering ange θ relative to as belows.
The sencond one is what is the angle of the beamforming? Is it 2*θ? Or is it other value?if it is other value,what is its value?
The third one is are the steering angle and the beam angle the same thing? If not,for different steering angle, the beam angle is the same,is that right?
The final question is about the computation of the tx phase shifter.There are 3 Tx antennas on the AWR1843 EVM,two azimuth antennas and one elevation antenna.When computing the phase shifter,the following formula is used:
where dx is defined in the following:
There are only two azimuth antennas on the AWR1843 EVM, Tx0 and Tx2,if I want to use beamforming ,I just need to configurate the two antenna, is that right? Or are the three antennas needed to set? If yes,how much should the dx value be?λ or 2λ?
Thanks,
Regards,
Rata