This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: IWR6843AOP demo not working (without breakaway board)

Part Number: IWR6843
Other Parts Discussed in Thread: AWR1843BOOST,

Hi,

I am having a similar issue as the problem described in here. I have flashed the AOP demo mentioned in that thread but when I try to run the AOP demo visualizer, the data port never connects as it is waiting for data (image below).

The problem might be that I removed the breakaway board so I am only using the radar part. Does the demo work correctly even without the breakaway board?

Also, I have tried flashing the area_scan demo (AOP binary) and running the MATLAB demo. It work once and after few seconds the demo stopped, the metal part was really hot. After that, every time I try to run the demo, a timout warning appears when sending the configuration parameters to the board.

What could I do to run the demo?

Thank you,

Ibai