Part Number: PGA411Q1EVM
hello I use the PGA411Q1EVM
for a project. in encoder mode can a phase shift be created between the mechanical and electrical angle of the motor. I get the u1, v1 and w1 signals on the ord0, ord2 and ord3.
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: PGA411Q1EVM
hello I use the PGA411Q1EVM
for a project. in encoder mode can a phase shift be created between the mechanical and electrical angle of the motor. I get the u1, v1 and w1 signals on the ord0, ord2 and ord3.
Thank you
Hi,
Does it mean that you want to have a delay when you read the angle information from u1, v1 and w1?
Regards
Sharath.
Hi
Yes .
sometimes the motor and the resolver do not have the same angle. I have to compensate electronically.
And aligne the output u ,v and w to the real u ,v and w of the motor.
I can do it mechanically but if it's possible with the board it will be great.
Thank you
Hi,
I dont think we have feature to delay the angle reading from the u,v, and w. Compensating electronically is the best options to these kinds of applications.
Regards
Sharath.
thank you
I want to make a phase shift between the reading of the resolver
and the U, V and W outputs on DRO0, DRO1 and DRO2
Hi,
Are you reading SPI register to read the resolver angle? I mean, what method are you using to read the resolver?
But, we dont have a mechanism to delay U,V and W outputs.
Regards
Sharath.