Hello TI team,
There are two questions I want to ask.
Now I can flash the FW through 2 RS232 pins without XDS110.
Q1: And I want to ask can I use the GUI " mmWave Demo Visualizer" through RS232 without XDS110? or any other method for using GUI without XDS110?
Q2: Can I flash the FW through the CAN transceiver? If not, how can I update the FW when the radar sensor has been fixed in the car?
Thanks,
Lukas