This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI team,
There are two questions I want to ask.
Now I can flash the FW through 2 RS232 pins without XDS110.
Q1: And I want to ask can I use the GUI " mmWave Demo Visualizer" through RS232 without XDS110? or any other method for using GUI without XDS110?
Q2: Can I flash the FW through the CAN transceiver? If not, how can I update the FW when the radar sensor has been fixed in the car?
Thanks,
Lukas
Hi
Question #1
Yes, it is possible to use the GUI through RS232. You will need a UART to USB converter to connect to the PC
Question #2
You would need a secondary bootloader in order to flash through CAN. We are in the process of releasing an example of that.
The example should be released in October/November time frame
thank you
Cesar