This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: mmwave demo visualizer connection issue

Part Number: AWR1843BOOST

Hello, expert.

Before I connected board to this visualizer, It was working well. 

But now days, I cannot connect to this visualizer. 

Board setting is (SOP = mode 4) functional mode. 

Its just commputer setting problem??

or board setting problem??? 

Thank you.

  • Hi heo je,

    So this issue might arise if the COM port is being utilized by some other application like tera term. Do check if while running the demo visualizer, the port isn't being utilized by another application. Also try the same with a different PC, with the same board and check if you are experiencing the same issue. As long as the port is isn't used by any other application this issue shouldn't arise.

    Regards,
    Saswat Kumar