Other Parts Discussed in Thread: AWR1843
The mmwave demo visualizer shows an angular resolution of 14.5 degrees.
Is this because the AWR1843BOOST antenna has a resolution of 14.5 degrees?
Also is there a way to change this number?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The mmwave demo visualizer shows an angular resolution of 14.5 degrees.
Is this because the AWR1843BOOST antenna has a resolution of 14.5 degrees?
Also is there a way to change this number?
Hi Yousuke-san,
Please find my responses to your questions as follows:
Is this because the AWR1843BOOST antenna has a resolution of 14.5 degrees? -> Yes
Also is there a way to change this number? -> This is based on the virtual antenna pattern of the AWR1843 and not a parameter that can be set as desired. 14.5 deg is the best resolution you can obtain; however, you can reduce the number of receiver channels and obtain lower resolutions (greater than 14.5 degrees).
For more details, you can refer to the following App note.
Regards,
Kaushik