Other Parts Discussed in Thread: AWR1843
Hello!
When using the ROS engine to generate mmWave point clouds, I noticed that the point cloud distribution forms an arc. Moreover, on the azimuthal plane, the spacing between points is very close, with an angular separation of approximately less than 2 degrees relative to the radar. However, to my knowledge, the azimuth angular resolution of the AWR1843 is only about 15 degrees. Why is it that when obtaining point clouds using the ROS engine, the angular separation between two points is 2 degrees? The same issue also occurs on the elevation plane.