This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
hi, engineers,
I studied the TI resource SWRA553A
Programming Chirp Parameters in TI Radar Devices (Rev. A)
for 2T4R mode, the angular resolution is 14.3°;
for AWR1843, TX0 and TX1 can work simultaneously when TDM-MIMO radar mode. TX1 and TX2 also.
but whether I can let TX0, TX1 and TX2 ,these three antennas work simultaneously, so that the angular resolution is 9.5° according to the formula below:
I just set two Tx successfully for their working simultaneously with mmwave Studio.
I want to improve angular resolution, especially for 3 TX work simultaneously.
Regards,
Wembanyama
Hi Wembanyama,
Refer to one of your previous thread to understand angular resolution - (+) AWR1843BOOST: angular resolution - Sensors forum - Sensors - TI E2E support forums.
Regards,
Samhitha