This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443BOOST: Accuracy

Part Number: IWR1443BOOST


Hi team,

I have checked mmWave level sensing video at https://training.ti.com/fluid-level-sensing-demonstration-using-ti-mmwave-sensors?cu=1135109
It stated that,  an accuracy of two to three millimeters can be achieved, up to 100 meters away with the use of a narrow field of view antenna.

Can you provide any use-case or simulation which achieves above accuracy up to 100 m.

Also, can you provide details of lens used in design: Fluid Level Transmitter with mmWave available at http://dev.ti.com/tirex/explore/node?node=ANSfP.znrAiHgDD7Sutxlw__VLyFKFf__LATEST

Thanks,

Akshay