Part Number: TDC1000-TDC7200EVM
Hi,
In another thread, I had explained how I was not getting consistent ToF measurements when the transducer was mounted on the outside wall of the container. While playing with two sensors to get differential ToF, immersed them in the medium (water) and then, placed them on the outside walls of the container. The ToF readings that started clocking inside the container continued even the two transducers were outside. Is this a restriction of the EVM that we have to start by placing the transducers inside the container? My application is for flow rate and the two transducers were to be mounted to the outside wall (non-intrusive). Kindly clarify this issue.
Regards,
A N Arunkumar