This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
I am trying to set up the Cascade RF board using the the "mmwave_studio_cascade_user_guide" document. In section 7.3.2 it says to select the Meta Image from the BSS FW Selection and click Load. When I use the file located at "C:\ti\mmwave_studio_02_00_00_02\rf_eval_firmware\radarss\xwr12xx_xwr14xx_radarss.bin" I get the following output from the console:
[15:39:11] [RadarAPI]: ar1.DownloadBssFwOvSPI_mult(1, C:\\ti\\mmwave_studio_02_00_00_02\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin)
[15:39:11] [RadarAPI]: Error: Download FW failed with error 64
Is this the correct FW file or am I missing something else here?
Thanks,
Robert
Cesar,
The link is on this page under the "MMWAVE STDUIO Cascade User Guide".
http://software-dl.ti.com/ra-processors/esd/MMWAVE-STUDIO/latest/index_FDS.html
Thanks,
Robert
Hi,
You also need to download the latest mmWave studio. The firmware included in "mmwave_studio_02_00_00_02" will not work
thank you
Cesar
Hi Cesar,
Using the 2.01 version of MMWave Studio and the 2.01 version of the firmware gives me the same error as before.
[RadarAPI]: ar1.DownloadBssFwOvSPI_mult(1, C:\\ti\\mmwave_studio_02_01_00_00\\rf_eval_firmware\\radarss\\xwr12xx_xwr14xx_radarss.bin)
[12:46:44] [RadarAPI]: Error: Download FW failed with error 64
Robert
Do you have a serial number for the boards you are using?
I have to check with our team which fw version would apply
Thank you
Cesar
The serial number for the DSP board is 003. I do not see a s/n anywhere on the RF board. Is there another label it is under?
Robert
Hi Robert,
Let me see if I can clarify some things here.
Please make sure to get the latest AWR1243 DFP package from: http://www.ti.com/tool/MMWAVE-DFP (DFP 1.2.5 is compatible with the mmWave Studio 2.1 release).
The Cascade Host board (MMWCAS-DSP-EVM) only supports loading the combined BSS/MSS "metaimage" binary on the AWRx devices. This is done using the ar1.DownloadBssFwOvSPI_mult() function as you called out. The problem is that you are pointing to the BSS binary, and not the metaimage binary.
I think this is confusing since we do not have a dedicated MetaImage loading function call, but rather re-utilize the BSS loading function call.
For DFP 1.2.5, after installation into the default path, the metaimage binary can be found here: C:\ti\mmwave_dfp_01_02_05_01\firmware\xwr12xx_metaImage.bin
The below lua script call would load in the metaimage from the default 1.2.5 install path:
ar1.DownloadBssFwOvSPI_mult(1, C:\\ti\\mmwave_dfp_01_02_05_01\\firmware\\xwr12xx_metaImage.bin)
We have also included a few example Cascade configuration scripts for reference to help new users get started. They are located here: C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Cascade
As a sanity check, I typically just run the C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Cascade\Cascade_Configuration_MIMO.lua script to verify everything is working.
The user guide has details on modifying that script to point to your MMWCAS-DSP-EVM over Ethernet and the local path to the DFP metaimage.
Please let me know if that solves your problem.
Thanks,
-Randy
Hi Randy,
Appreciate the post on the forum. It did get me past the error I was having, but I later hit a snag using the GUI setup when triggering a frame. There is a line in the guide that states that "The other configuration API’s are similar to the sequence followed in single chip apart from the frame configuration," which I was unclear on. Do I need to follow the guide for setting up a single chip for this part?
I also tried to run the lua script you mentioned and got the following error:
"\Lua\5.1\lua.exe: ...tudio\Scripts\Cascade\Cascade_Configuration_MIMO.lua:517: attempt to call global 'WriteToLog' (a nil value)stack traceback: ...tudio\Scripts\Cascade\Cascade_Configuration_MIMO.lua:517: in main chunk"
I have never used lua before, but am running the script from the command line once the board is powered on and the cascade option is selected in MMWave Studio. Please let me know if I am doing that wrong or if there is a different way I need to be running the script.
Thanks again for the help,
Robert
Hi Robert,
I think there is some confusion here. The example lua scripts are meant to be run from within the mmWave Studio GUI itself. I do not think you can run these from the lua interpreter directly on the command line since these scripts expect additional lua dependancies which the Studio GUI provides.
To run these scripts, use the lua script run command and text input box at the bottom of the GUI. The script that is to the right of the "Run!" button will be executed when you hit "Run!".
Can you also please verify, when you installed mmWave Studio 2.1, did you install all of the runtime dependencies as well? These are listed in the mmWave Studio User Guide. http://software-dl.ti.com/ra-processors/esd/MMWAVE-STUDIO/latest/exports/mmwave_studio_user_guide.pdf. See the section 2.1 "Installation" for details.
Can you please try it through that script run interface in the GUI and let me know if you see any problems?
Regarding your frame triggering question, the Cascade_Capture.lua script provides an example of setting up the TDA2x host processor and the AWRx master and slave devices for capture and triggering the capture. It will be in that same script example path: C:\ti\mmwave_studio_02_01_00_00\mmWaveStudio\Scripts\Cascade\Cascade_Capture.lua
You can use the GUI buttons to run through all of those steps, but I do not recommend it. I recommend just setting up a config and capture script like the example scripts provided.
The cascade capture sequence can be summarized as: