This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello all,
I have been recording with IWR6843ISK + MMWAVEICBOOST+ DCA1000EVM and processing everything with mmWaveStudio solution. Now, I changed and started a signal processing on Matlab using the adcData.bin file is dumped from the recording and the readDCA1000 function you provide. The issue is that every other index in the file is null or 0, and I am not sure what it can be wrong, since it worked for the mmWaveStudio GUI. I have attached an example of several that I have taken, all of them resulting in the same problem. My configuration is:
Please find attached the configuration and output images. I want to record in a really short range with high resolution, the reason why I have set this way the parameters.
Thank you,
Gorka Iturbe
Hi,
In your LVDS lane configure, you should have Lane 1 and Lane 2 both checked by default. Why you have only lane 1 checked?
Best,
Zigang