This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Beam switching between frames

Part Number: IWR6843

Hi,

Two quick questions regarding TX beam forming/beam steering in 6843 chip:

1- Is it possible to switch beam (or phase of channels) between frames?

2- How fast we can do beam switch (in terms of us, ms or in terms of fps)? 

Thanks

  • Hi Nimo,

    I've asked an expert to look into this and we should have an answer for you in the next few days.

     

    Cheers,

    Akash

  • Hi, there:

    Yes, the mmWave SDK support per profile based beam steering, and up to 4 subframes.  You can program different beam steering for different subframe. 

    An example for sub frame configuration is given below.  You can search each command details inside the mmWave SDK users guide at C:\ti\mmwave_sdk_03_03_00_03\docs\mmwave_sdk_user_guide.pdf

    profileCfg 0 61.0 10 6 135 0 14970880 2.5 1 256 2000 0 0 48
    profileCfg 1 61.0 10 6 135 0 10276864 2.5 1 256 2000 0 0 48
    profileCfg 2 61.0 10 6 135 0 6565888 2.5 1 256 2000 0 0 48
    profileCfg 3 61.0 10 6 135 0 1871872 2.5 1 256 2000 0 0 48
    chirpCfg 0 0 0 0 0 0 0 7
    chirpCfg 1 1 1 0 0 0 0 7
    chirpCfg 2 2 2 0 0 0 0 7
    chirpCfg 3 3 3 0 0 0 0 7
    advFrameCfg 4 0 0 1 0
    subFrameCfg 0 0 0 1 128 80 0 1 1 80
    subFrameCfg 1 0 1 1 128 80 0 1 1 80
    subFrameCfg 2 0 2 1 128 80 0 1 1 80
    subFrameCfg 3 0 3 1 128 80 0 1 1 80

    In the example above, different profile is given different phase shifting angle (marked in red), and all 3 TX antenna are transmit at the same time to achieve the beam steering.   

    The subframe period is set to 80ms in the above example.  You can modify the subframe periodicity to switch faster between sub-frames. 

    Another method is per chirp phase shifting.   You can program different chirp steering at different beam angle within one frame.  But then the Doppler FFT have to change for this type of configuration, that is why it is not supported yet in mmwave SDK.   But you can use DCA1000 + radar studio to do raw data capture using this mode and do post processing offline. 

    Best,

    Zigang

  • Awesome,

    Thank you for your quick response.

    Very helpful