This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642BOOST: CANFD_init() appears stuck

Part Number: IWR1642BOOST


Tool/software: Code Composer Studio

it seems that this code appears to work on all devices, but fails some of the time causing the device to appear locked up.When i connect Kvaser Leaf Light v2 with devices,it will resturns .And MCAN can send messages ot.But when i disconnect can communication,the code appears to be in dead cycle新建 Microsoft Word 文档.docx.

  • Interesting.  I have not heard of that happening.  A few questions:

    1) Does it hang when you boot up with nothing connected?

    2) Does it hang if you leave the external device connected (without disconnecting while in use)?

    3) If you have access to another EVM, does it do the same thing?

      -dave