Other Parts Discussed in Thread: MMWAVEICBOOST
Hi,
I was able to connect the IWR6843AOPEVM to the MMWAVEICBOOST and DCA1000 to get raw data off the device.
Now, I would like to connect the IWR6843AOPEVM to my own custom hardware (using the same high density connector used with MMWAVEICBOOST) to live stream raw ADC data into my hardware. Is there any documentation on the high density connector and how it can be connected to custom hardware? I did run into ticket (https://e2e.ti.com/support/sensors/f/1023/t/782341) which was asking a very similar question about getting the raw data without using DCA1000 but looks like it was resolved through direct communication with the ticket creator and I am unable to determine how that issue was resolved.
Any help you can provide on getting the raw data into my hardware, using the IWR6843AOPEVM board would be greatly appreciated.
Cheers,