I have AWR1843Boost EVM rev C. I have few questions:
1. I am trying the beam steering example given by TI, I am not getting any data in y-z plane or Elevation, any help will be appreciated. The pdf in that example says that, to use the third Tx antenna 1V supply is required and for that a 0Ohm resistor is to be mounted but that is for Rev A, and I have Rev C that comes with 1V supply, I believe, correct me if I am wrong, otherwise please help me to obtain the data in elevation.
2. Regarding the angular coverage of this device, what is the elevation range, as it is not mentioned in the documents?
3. Is there any example to achieve 250m range, as the datasheet says this device can have a max range of 250m?