This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: High Accuracy Visualizer - Range Profile - unit of the Y axis

Part Number: IWR6843AOPEVM


Hello, I did some labs with 

- High_Accuracy_Visualizer 1.2.0
- IWR6843AOPEVM ES2
- mmWave SDK: 03.04.00.03
- IWR toolbox 4.3.1 http://dev.ti.com/tirex/explore/node?node=AOKFXTJ05qLZ2hdDXQ1E8Q__VLyFKFf__LATEST

What is the unit of the Y axis in the Range Profile plot? (Is it 'dB' like the mmWave_Demo_Visualizer_3_4 3.4.0?)
I found out that the value is proportional to 'chirps per frame'...

related question: What is the unit of the "logMagRange" data send over DataPort for the rangeProfile?

best regards, Ruben