Hi,
I'm trying to understand the calibration step of the EVM with mmwave studio. The calibration is done for 12 Tx and 16 Rx. Would the generated calibration matrix work for transmitters less than 12 or receivers less than 16 or do we have to calibrate again with the new setup? I'm disabling the number of transmitters and receivers by disabling the number of chips in the cascade board The procedure says to refer to "signal_processing_4chip_cascade.pdf" (as shown) if I have questions about Antenna Calibration. However, there's no such file present in the mmwave studio installation folder.
Can someone explain the first question and (if possible) attach the concerned PDF? Thank you.