This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/IWR1642: Unable to get 16xx - mmWave SDK Demo project to load in CCS

Part Number: IWR1642

Tool/software: Code Composer Studio

In the user's guide page 10, step 2, neither the MSS nor DSS projects can be imported, instead I get a message "To look at the project source files, please import he project in CCS following the instructions provided in the user guide." I must be following the wrong user guide? I have tried the latest version of the industrial toolbox, V4.3.0, and V2.0.0. V2.0.0 allows me to load the project, but I get errors with paths not being valid.

  • Looks like you have to do the following to import the MSS and DSS projects.

    Once you are in CCS right click in the Project Explorer: Import -> CCS Projects:

    Then use the following path:

    <Industrial Toolbox Install Path>\labs\out_of_box_demo\16xx_mmwave_sdk

    This should import both mss and dss projects into the CCS Project Explorer.

    Building/compiling is another story after getting the projects imported.

  • Hi Clint,

    I'm glad you were able to resolve it. If you still have questions feel free to open up a new thread.

    Regards,

    AG