Other Parts Discussed in Thread: AWR1642
Hi
1) I am learning TI mmwave sensors using AWR1642BOOST (ES2.0) + DCA1000 EVM with a Windows 10 laptop and mmwave Studio 02.01.01.00. I am collecting 2x complex data from the ADC.
I refer "numAdcSamples" variable at location file:///C:/ti/mmwave_sdk_03_03_00_03/packages/ti/control/mmwavelink/docs/doxygen/html/structrl_profile_cfg__t.html
It states that : Valid range: 2 to MAX_NUM_SAMPLES
However, in mmwave Studio tab " SensorConfig" , I found that I cannot set number of ADC samples less than 64. Please advise how can I set the number of ADC samples less than 64 in mmwave Studio 2.1.1.0. I particular, I wish to set the number of ADC samples to 8 or 4 or 2.
I have been advised earlier by TI team that earlier there was a limitation that ADC samples could not be set less than 64 in mmwave Studio, however, this limitation has been removed in mmwave Studio 2.1.1.0 and now ADC samples could be set as low as 2 in mmwave Studio 2.1.1.0. ( https://e2e.ti.com/support/sensors/f/1023/t/912349 message dated 22 June, 2020)
However, I found that even mmwave studio 2.1.1.0 , I cannot set ADC samples (in SensorConfig tab) less than 64. This is the same limitation that we had in mmwave Studio 2.0.0.2.
Please advise how can I set number of ADC samples as low as 2 (or 4 or 8) in mmwave studio 2.1.1.0 ?
2) I wish to set the start the Tx frequency as 77 GHz and I wish to experiment with very short bandwidth, say 90 MHz or even less. Please advise how can I set this bandwidth (90 MHz or even lower) in mmwave Studio 2.1.1.0 ? Should I set it in tab " StaticConfig " of mmwave Studio 2.1.1.0 ? Or is there some other way to set the bandwidth of Tx signal ?
Please also advise that is there any lower limit of bandwidth that could be set for Tx signal ? If yes, then please advise TI document(s) stating that limit for the AWR1642 device, for TI Demo Visualizer and for mmwave Studio 2.1.1.0.
Thanks and regards