This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK-ODS: GUI People Counting issue

Part Number: IWR6843ISK-ODS
Other Parts Discussed in Thread: MMWAVEICBOOST, IWR6843

Hi everyone,

I have some trubbles to run the People Counting demo. 

  • Sensor = IWR6843 + MMWAVEICBOOST
  • Toolbox = 4_3_2
  • Lab = Long Range People Detection with BeamForming

My goal is to correctly use the BeamForming.

However, once the sensor is flashed with the lab Long Range People Detection 4_3_2 and connected to the app, I am not able to select or send a configuration and disconnect the radar neither. It seems that the buttons are linked to nothing...

If I try to use the toolbox 4_1_0 (demo + lab flashed) everything seems working well.

I downloaded the latest SDK(version 03_04_00_03) but I have 3 or 4 several SDK installed in my computer and I wonder if the people counting vizualiser is looking for the good SDK version ? How could I verify that ? Do I have something to do to disable older SDK ? 

Maybe my problem is not linked to the sdk but I have no other idea.

I already spoke about my issue on another post but it was not in the good forum :

e2e.ti.com/.../3395668

Thanks by advanced,

have a good day