Hello, the engineers of TI!
After using the IWR6843ISK-ODS to get some datas, I did the following steps of data processing:
First, a FFT algorithm is used for matching filtering.
Second, a MTI algorithm is used for removing the static clutter, and MTI algorithm is realized by subtracting adjacent pulses.
The problem is that after MTI, some bright lines would appear in the time-distance image, and the gap of the adjacent bright lines was a constant, and the constant is the same as the number of cycles per frame set in the acquisition software(MMwave studio).