This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: Setting range of txOutPowerBackoffCode

Part Number: IWR1443


What is the range of values that can be set for txOutPowerBackoffCode?
Is it possible to set -30dB?
When I check the waveform of rangeProfile with Visualizer, I can see the difference in relative power between -9dB and -12dB.
However, there is no difference in relative power between -12dB and -30dB.

Best Regards,
Hiroyuki taguchi