Other Parts Discussed in Thread: IWR6843
Tool/software: Code Composer Studio
Hi,
I use the IWR6843 AOP ES2.0, with toolbox 4.4.1,
1) is the "RX channel phase compensation" step for this device is "file:///C:/ti/mmwave_sdk_03_04_00_03/packages/ti/demo/xwr64xx/mmw/docs/doxygen/html/index.html#Calibration_section", rather than "file:///C:/ti/mmwave_sdk_03_04_00_03/packages/ti/demo/xwr68xx/mmw/docs/doxygen/html/index.html#Calibration_section"?
2) is the "RX channel phase compensation" step means that once I get the "RX channel phase compensation" , i can use it no matter what changes to make to the profile ?
In another words, If I get the "RX channel phase compensation" use this step, can I use it when I use the "long range people detect" with my new profile, or I have to make the new "RX channel phase compensation" use this step.
when I use the "file:///C:/ti/mmwave_sdk_03_04_00_03/packages/ti/demo/xwr64xx/mmw/docs/doxygen/html/index.html#Calibration_section"
I can get the factor with almost no change, or changes very little.
But when I use my ""long range people detect" Demo , with my profile, use TX Beamforming, I use my project just chagne the "measureRangeBiasAndRxChanPhase" configuration, and make it output the
factors, but the output changes as following:
compRangeBiasAndRxChanPhase -1.3608793 0.36844 0.31931 0.55060 0.75287 -0.50229 0.26788 -0.81372 0.58124 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.9612230 0.18130 0.17618 0.60263 0.60263 -0.33115 0.12375 -0.96353 -0.26764 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0121234 -0.35559 0.29599 -0.74899 -0.66257 -0.28220 -0.56830 -0.07532 -0.59238 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0820955 -0.04208 0.03537 -0.35114 -0.93634 -0.01462 -0.04242 0.03571 -0.05286 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.1955293 -0.21426 -0.24167 -0.76428 -0.64487 0.15613 -0.30389 0.24298 -0.30463 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2479240 0.11548 0.29391 0.00000 0.99997 -0.30838 -0.09277 -0.18686 -0.78140 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.3949114 -0.14682 -0.41895 0.90848 0.41791 0.32373 -0.50873 0.47769 -0.18631 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2583014 -0.13123 -0.12646 -0.97342 -0.22903 0.13568 -0.06366 0.20380 0.04907 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2465762 -0.00552 -0.00690 0.70709 0.70709 0.00595 -0.01111 0.00711 -0.01031 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2171067 -0.19327 0.11075 -0.91916 0.39392 0.19077 -0.30298 0.24615 0.67133 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0144897 0.18741 0.19989 -0.05548 0.99847 -0.27512 0.20364 -0.36017 0.01199 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.4615811 -0.10703 -0.10480 -0.44720 0.89444 0.17300 -0.08197 0.33655 0.15799 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2305220 -0.15186 -0.17007 0.11685 -0.99316 0.17557 -0.35114 0.25702 -0.35983 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.4151478 -0.11298 -0.13931 0.93634 0.35114 0.06189 -0.30383 -0.04425 -0.30426 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0942679 0.27405 0.28305 -0.04645 0.99893 -0.34125 0.22046 -0.47714 0.04266 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase -0.0742530 0.04037 0.03339 0.70709 0.70709 -0.03427 0.02332 -0.05820 -0.02850 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase -0.0316231 0.19705 0.18256 0.48065 0.62308 -0.36560 0.26114 -0.94867 0.31622 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase -0.1543153 -0.13690 0.11130 -0.55124 -0.08972 0.03870 -0.23950 0.16440 0.98639 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 9.8216839 -0.34589 -0.36920 0.66812 0.74405 0.10043 -0.45871 0.45587 -0.42081 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase -0.0487351 -0.19104 0.11887 0.44720 -0.89444 0.01782 -0.21274 0.27692 -0.16614 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2072534 -0.18768 -0.25247 0.47409 -0.88046 0.39496 -0.32422 0.31610 -0.30313 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.4025639 -0.03912 -0.11935 0.99228 -0.12402 0.25183 0.24420 0.49612 -0.86826 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0609625 -0.20404 0.28604 -0.76154 -0.64813 -0.40118 -0.32010 -0.30450 -0.41025 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.2707365 -0.16946 -0.15909 0.01868 0.31128 0.19952 -0.42758 0.64020 -0.76822 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0514474 0.17831 0.26025 0.12106 0.99265 -0.50275 0.11603 -0.88010 0.26608 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0525093 -0.10892 0.16736 -0.40823 0.74442 -0.16840 -0.32352 -0.86618 0.49973 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
compRangeBiasAndRxChanPhase 0.0844054 -0.15567 -0.20038 0.74210 -0.67029 0.17316 -0.13504 0.19772 -0.03168 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000 0.00000
then which one should I use?
a) use the factor generate with the profile "C:\ti\mmwave_sdk_03_04_00_03\packages\ti\demo\xwr64xx\mmw\profiles\profile_calibration.cfg" and bin "C:\ti\mmwave_sdk_03_04_00_03\packages\ti\demo\xwr64xx\mmw\xwr64xxAOP_mmw_demo.bin";
this factor is almost the same.
b) use the factor generate with the my own profile and my changed "long range people detect " Demo project with the AOP device and TX Beamforming?
this factor is changed periodic;
If I use the type b), then which factor should I use?
3) does the AOP's TX beamforming have effect to the compRangeBiasAndRxChanPhase?
thank you very much!