This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Which value can I use as ADC sampling rate?

Part Number: AWR1843

Hello.

I have used profileCfg below and I want to halve maximum range and number of sample.

profileCfg 0 77 7 7 58 0 0 68 1 128 2750 0 0 30


I tried to use profileCfg below, but this command couldn't be used.

profileCfg 0 77 7 7 58 0 0 68 1 64 1375 0 0 30


I think number of sample "64" is no problem, so error point is ADC sample rate "1375".

In user guide, sample rate  is "any value as per mmwavelink doxgen/device datasheet".

I checked "C:\ti\mmwave_sdk_03_01_01_02\packages\ti\demo\xwr18xx\mmw\docs\doxygen\html\index.html" and other pages,
but I can't find the information I want.

How can I know valid ADC sample rate?

BR,
Nobu