This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: Out of box demo does not start

Part Number: IWR6843AOP

Hi,

I have recently bought IWR6843AOP chip:

We have tested that Out of Box demo for IWR6843AOPEVM 2.0 works as expected and after applying the same code to the custom board with the chip specified above, I was not able to produce the same working results. The code crashes after it tries to talk with the chip and the hardware itself (custom one) works as expected (we can debug using XDS, UART and etc.). This behaviour occurs using mmWave SDK 3.4 and Industrial Toolbox 4.4.0

We have also tried to do the same with SDK 3.5 and Toolbox 4.5.1, it did not crash but we were not able to see any results as the GUI for mmwave radar does not support SDK 3.5

Here is the schematic for the radar:

Radar.pdf

What could be wrong?