Hello,
We are using the OPT3002 to detect the illuminance of the green LED.
After firing the green LED for about 200 hours, we measured the output of the OPT3002 and found that the value increased by about 2% from the initial value.
(Supplementally, the OPT3002 has been exposed to green LED light throughout this test.)
Then, when we measured the irradiance of the green LED, the irradiance of the green LED was reduced by about 2% from the initial value.
(See the graph below.)
Normally, the output of the OPT3002 should decrease as the LED irradiance decreases, so we are wondering about this result.
So we want you to tell us the following:
1. Is the output of the OPT3002 likely to change after long-term use even if the amount of light received is constant?
2. Can the spectral response of the OPT3002 change after long-term use?
3. If questions 1 and 2 are no, do you know another reasoning that can explain our test results?
4. Please tell me how to use OPT3002 well to keep the error between OPT3002 output and irradiance small.
Best regards.