Other Parts Discussed in Thread: MMWAVEICBOOST,
Hello,
I use an IWR6843ISK ES2.0 in combination with the MMWAVEICBOOST and CCS 10.1.1.00004 with the mmwave_industrial_toolbox_4_5_1 and mmwave_sdk_03_05_00_04.
I tried the CAN test code from
C:\ti\mmwave_sdk_03_05_00_04\packages\ti\drivers\canfd\test\xwr68xx\main.c
but if fails with these errors:
It seems that there is a problem with XDCtools, I am using the 3.61.2.27_core:
Is the CAN test program compatible with this XDCtools core version?
Is there any solution to fix this error?
Thank you!