Hello,
i am working with the IWR6843ISK on the MMWAVEICBOOST.
I used the Adding CAN-FD Tx and Rx to an Existing mmWave Project to add CAN to the gesture recognition program, prevented by the code composer studio industrial toolbox 4.5.1.
But for the function
canHandle = CANFD_init(&mcanCfgParams, &errCode);
i get the error:
Description Resource Path Location Type
#167 too few arguments in function call mss_main.c /multi_gesture_68xx_ods_mss/mss line 1971 C/C++ Problem
Can someone explain how to fix this problem?
Thank you.
Thank you for your help.