This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
When i read the function of MmwDemo_dataPathConfigBuffer,i have a question.
If we use demo11 about MRR && USRR,and we use two subFrame.When we alloc L2 memory about part2,for example twiddle16×16_1D.
According to the code, obj will be increased during MRR && USRR memory allocation, but obj will point to the same memory space address, that is, USRR twiddle16×16_1D will overwrite the memory space of MRR twiddle16×16_1D.
Or did I misunderstand the code? Please ask TI engineers to confirm the following.
Thanks a lot!
Bryant
Hello,Cesar
Thank youi very much!
I have another question.Does AWR1843 have HSRAM.I remember AWR1642 have a HandShake Ram which size is 32K.
If memory is not enough,can i use HWA M0~M3 to be memory?What are M0~M3 respective sizes?16K each?
Thanks a lot!
Bryant
Hello,Cesar
Can HWA memory be read and written directly by address?It's on the same address bus as L1/L2/L3, right?Are reads and writes slower than L1/L2/L3?
Thanks a lot!
Bryant
Hello,Cesar
Today i use ccs and awr1843boost and i want to use address to read and write the HWA memory,and i find that hwa memory can not be write,and when i read the memory,it is dirty.
Do I need to enable the HWA hardware function before I can read and write the HWA memory address?Are HWA memory addresses set to read and write permissions?
Thanks a lot!
Bryant
Did you try to write/read the HWA memory with CCS or with C code?
You should try with C code
thank you
Cesar