Hello,
I have used the LMT70EVM before on my system and faced no issues two yers back. But when I tried testing the evaluation kit now, it doesn;t respond and I could see that the LEDs D1 and D2 are also not responding while connecting the board to my PC. I verified the following:
(1) Checked the Driver file path
(2) Verified the COM port number
(3) Verified the power on the board
(4) Scanned for latest driver for the COM port
I followed the instructions in the LMT70EVM Quick reference guide. Checks listed above looks good except that I couldn't access the Board from system using LMT70EVM desktop app and couldn't find the device on MSP430 USB firmware upgrade tool.
I have included screenshots of the issue below for further clarity. It seems like the Mixed-Signal Microcontroller (Part U3 on the Board) doesn't respond.
Please review and advise me regarding this concern.
Best Regards,
Nandhini Jayapandian