This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: awr1243boost revA

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: DCA1000EVM, , AWR1243

My device is awr1243boost rev. A. It's connected to dca1000evm. When running mmwavelink_example.exe, I got "mmWave Device Power On failed with error -8".

Mannually pushing RESET button wouldn't help. But using mmWaveStudio is Okay.

I guess the reason is that the provided mmwlstudio.lib in DFP isn't correct. I hope you can verify that.

Besides, in the documents of DFP, awr1243boost is connected to DevPack rather than DCA1000EVM. Could that be the reason why mmwavelink_example.exe didn't work?