This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1612: Moisture sensitivity and target material

Part Number: LDC1612

My customer has additional questions:


- is the inductive measurement with the LDC sensor and PCB integrated coil sensitive to moisture?

If so, you can provide me with data.

What is the intensity of moisture that causes what change or is it independent of moisture?

Compensation is not possible for us, because we have not designed in a humidity sensor.

- Which material / steel types would you recommend to us to tune the coil ideally?

So what material should ideally be used for our spiral spring.

Best regards

Egon

  • Hi Egon,

    The Moisture Sensitivity Level of the LDC1612 can be found in the Packing Information section of the datasheet. All LDC1612 orderable devices have an MSL rating of 1, which is considered not moisture sensitive at 85% relative humidity. Please refer to MSL Ratings and Reflow Profiles for more detailed information.

    Regarding the target material, any metal can be used as a target, but more conductive materials will give stronger inductive responses. It is recommended to use highly conductive targets such as copper or aluminum. Further information about this can be found in LDC Target Design.

    Best regards,

    Nicole

  • Hello Nicole,

    the question about the moisture sensitivity is not related to our LDC1612, it's related to the value of the coil.

    Best regards

    Egon

  • Hello Egon,

    My apologies on this.

    Unfortunately, we don't have data regarding the effect of moisture on inductance measurements. It may be possible that certain coil properties change with added moisture in the environment, but this will be hard to quantify.

    Best regards,

    Nicole