Part Number: PGA305EVM-034
Hi sir,
A customer is using TI PGA305 EVM board, he have a query on ADC sampling rate.
In regards to the 1024 us sampling rate,
if I wanted to sample at 10 -15 Hz , is the ADC sampling rate still fixed at 1024 us?
or does this decrease with frequency? Our use case may work with the sampling rate of 1024 us,
but we are not sure if the same sampling rate is constant when we work in the 10 - 15 Hz ranges.
Thanks for your clarification.
Regards,