This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: AWR1843BOOST

Part Number: AWR1843BOOST

Hi everyone,

Please I am trying to  enable 3 TX and 4 RX  using my 6843aop with dca100 and AWR1843BOOST  for ADC data collection The setting works for only when 2 TX is enabled.

% ***************************************************************
% Created for SDK ver:03.05
% Created using Visualizer ver:3.5.0.0
% Frequency:60
% Platform:xWR68xx
% Scene Classifier:best_range_res
% Azimuth Resolution(deg):15
% Range Resolution(m):0.044
% Maximum unambiguous Range(m):9.02
% Maximum Radial Velocity(m/s):1
% Radial velocity resolution(m/s):0.13
% Frame Duration(msec):100
% RF calibration data:None
% Range Detection Threshold (dB):15
% Doppler Detection Threshold (dB):15
% Range Peak Grouping:enabled
% Doppler Peak Grouping:enabled
% Static clutter removal:disabled
% Angle of Arrival FoV: Full FoV
% Range FoV: Full FoV
% Doppler FoV: Full FoV
% ***************************************************************
sensorStop
flushCfg
dfeDataOutputMode 1
%channelCfg 15 5 0
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg -1 0 1 1 1
profileCfg 0 60 3.4 0.2 26.6 0 0 150 1 262 10000 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
chirpCfg 2 2 0 0 0 0 0 2
frameCfg 0 1 16 5400 1000 1 0
lowPower 0 0
guiMonitor -1 1 1 0 0 0 1
cfarCfg -1 0 2 8 4 3 0 15 1
cfarCfg -1 1 0 4 2 3 1 15 1
multiObjBeamForming -1 1 0.5
clutterRemoval -1 0
calibDcRangeSig -1 0 -5 8 256
extendedMaxVelocity -1 0
bpmCfg -1 0 0 1
%lvdsStreamCfg -1 0 0 0
lvdsStreamCfg -1 0 1 0
%lvdsStreamCfg -1 0 0 1
compRangeBiasAndRxChanPhase 0.0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0 1 0
measureRangeBiasAndRxChanPhase 0 1.5 0.2
CQRxSatMonitor 0 3 5 121 0
CQSigImgMonitor 0 127 4
analogMonitor 0 0
aoaFovCfg -1 -90 90 -90 90
cfarFovCfg -1 0 0 8.92
cfarFovCfg -1 1 -1 1.00
calibData 0 0 0
sensorStart

  • Ukeme,

    I would suggest reviewing the frameCfg argument that you provided:

    frameCfg 0 1 16 5400 1000 1 0

    This command will only utilize chirps 0 and 1. If you want to utilize all three chirps, and by extension all three TX antennas, the argument should be:

    frameCfg 0 2 16 5400 1000 1 0

    There is plenty of interframe margin when enabling the third transmitter.

     

    Regards,
    Kyle