This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: Not working with IWR6843ISK

Genius 9880 points
Part Number: DCA1000EVM


Hi Team,

According to customer, the DCA1000EVM not working and want to know how to repair  or it is possible to refund it.

Below are the details.

"

1. When received the EVM, it does work?
    --> When I received it, it was working. But not now.
 
2. If yes, when was the last time you used the EVM when you encountered that it is not working?
    --> I have used EVM successfully several times up to about 2 month ago. But not working now.
 
3. What is your test setup when the EVM did not work?
     --> It was used to download the data from IWR8843ISK EVM (60 GHz mm-wave radar sensor). The setup is general, which means just connection with cable.
          and powering by PC. That's it. No other specific ones.
4. Any helpful information to help us troubleshoot the EVM would be much appreciated.
    --> I want to ask you to check the board and repair it if there is a problem.
"
Thank you and looking forward for your kind response.
Regards,
Maynard