This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,ti's rngineers
I read the AWR1843 DEMO7(MRR),i find tow functions and i can not understand them.
The function of computeSinAzimSNR calculate the SNR about obj's azimuth snr, and the function of convertSNRLinToVar calculate the variance about obj's azimuth,what's the theory behind this?In what reference books can I find all this theoretical knowledge?
BR
Bryant
Hi Bryant,
computeSinAzimSNR - computes SNR of a tone in a 'zero padded FFT' - by essentially defining SNR as the ratio of the peak and sum of the energy of at the expected locations of the nulls (if the signal was a pure sinusoid).
As an example, create in matlab a complex sinusoid of length 4 (say of an arbitrary frequency), and construct a 64 pt FFT of the signal, and plot the absolute value of the FFT output. You would notice that the nulls correspond to points at an offset of 16 ( or 64 / 4) from the peak. If the input signal is noisy (i.e. gaussian noise) , these nulls locations would no longer be nulls, would have some noisy energy. Hence the ratio would correspond to the SNR measurement.
convertSNRLinToVar assumes that given an SNR of an estimate (and knowledge that your estimation algorithm is equivalent to maximum likelihood), you can estimate the expected variance of the estimate (by inverting the Cramer Rao Bound - as the equation to convert from SNR to variance). You can read up on CRB in Fundamentals of Statistical Signal Processing: Estimation Theory by Steven M. Kay.
Regards
Anil
Hi Anil,
In function about convertSNRdBToVar,the invSNRlin is invSNRlin = antilog2(-SNRdB, bitW) * 2;
In function about convertSNRLinToVar, the invSNRlin is recipsp( (float) SNRLin) * ((float) (1 << bitW));
Why the invSNRlin is different?Is there any theoretical calculation formula behind INVSNRLIN?
Regards
Bryant
Hello,Anil
You says"create in matlab a complex sinusoid of length 4 (say of an arbitrary frequency), and construct a 64 pt FFT of the signal",do these four points need to be included in a complete period?Or are these four points any four points, not a complete period?
BR
Bryant