Other Parts Discussed in Thread: DCA1000EVM
Hi,
using Win10, I installed mmWStudio 3.0.0.14. During the startup (behind the splash screen), I always get a window opening with an error message:
Seems a file is crashed or missing. Has anybody got a name, an address ( :-) )? Where can it be found?
At the end of the day, this installation will at least execute the script, open the Radar API and connect the FTDI chips, but no device is detected and no RS and SPI connection can be done.
No visible change to the USB devices takes place.
(In contrast to a Win7 installation on another machine, where additional USB devices pop up, but there the MATLAB stuff won't run due to a 64-32 bit incompatibility, some DLL is not found and the script won't terminate so I cannot check if connections could be made there)
Thanks