This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: May I know IWR1843, IWR1443, IWR1642 detection distance and what is the detection distance accuracy ?

Part Number: IWR1843
Other Parts Discussed in Thread: IWR1642, IWR1443

Hi 

Have a good day.

May I know IWR1843, IWR1443, IWR1642 detection distance and what is the detection distance accuracy ?

  • Hi Jian

    All of these devices have capability to detect objects more than 100m out and also with capability to detect nearer objects with millimeter accuracy. This will depend on the application and how the sensor is used. Can you provide more information about the application?

    Regards,

    AG