This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I cannot communicate with the sensor. Using UNIFLASH, I get the error "Not able to connect to serial port. Recheck the COM port selected.".
When I power on the board, the led D7 turns on "lightly" (according to the figure) . I think that in a normal situation this would not happen.
I already tried this operation with different OS (Linux and Windows) and different cables.
Any suggestion?
Best regards,
--
Guilherme Amaral
Hello,
I will need some more information. Can you please ensure that you have set the SOP switches correctly as in this page: https://dev.ti.com/tirex/explore/content/mmwave_industrial_toolbox_4_7_0/labs/common/docs/hardware_setup/hw_setup_isk_ods_modular_mode_flashing.html
Are you connecting to the correct USB ports as described in this page: https://dev.ti.com/tirex/explore/content/mmwave_industrial_toolbox_4_7_0/labs/common/docs/software_setup/using_uniflash_with_mmwave.html
Hello Sabeeh,
Yes, the SOP switches are:
S1.1 - ON
S1.2 - OFF
S1.3 - ON
S1.4 - ON
S1.5 - OFF
S1.6 - N/A
The USB ports are identified by the OS. I had done the operation before, following the same procedure, and it worked.
Is it normal for the D7 led to be like this?
Thanks in advance! Best regards,
--
Guilherme
Sabeeh,
Note that the LED (D7) doesn't have the intensity of the others. It has a very low intensity!
So... If it is not a problem, do you have any idea why I can't communicate with the sensor?
Have you installed the correct drivers? https://www.silabs.com/products/development-tools/software/usb-to-uart-bridge-vcp-drivers
Yes I did! As I mentioned, I had never had any problems with communication before.
Have you tried doing a full power off/on of both the PC and sensor?
If there is an image currently flashed on to the device, are you able to get that working? In other words, put the device back into functional mode and test the application already on the device. This will atleast determine that there is nothing wrong with the hardware.
I already made all the suggestions you presented before asking the question here. The firmware on the board is not working. The sensor doesn't respond
What does the sensor do when you try to send it a *.cfg file from the Out of box demo visualizer? Link: https://dev.ti.com/gallery/view/mmwave/mmWave_Demo_Visualizer/ver/3.5.0/
Do you happen to have a mmWaveICBOOST? I would kindly ask you to connect the sensor to the ICBOOST and use the ICBOOST for communication. Doing this bypasses the CP chip (USB-UART transceiver) on the ISK and uses the XDS110 on the ICBOOST.
If there is truly no response then it seems to me that you have a broken sensor and can (depending on time from purchase) qualify for a replacement. Please contact TI support and link to this E2E thread.