This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843: Nothing displays in demo visualizer

Part Number: IWR6843

Hello,

I am doing MMWave SDK Demo-68xx DSP Version. I am using IWR6843ISK. It is placed at a height f 2.3m from ground and with a tilt of 10 degree. i have followed the steps in file:///C:/ti/mmwave_industrial_toolbox_4_7_0/labs/out_of_box_demo/68xx_mmwave_sdk_dsp/docs/mmWave_sdk_68xx_dsp_user_guide.html. After running the visualizer nothing happens in the plot. Ports were succesfully connected.

  

Please help me to resolve this.

Thanks and Regards,

Aleena N A

  • Hi Aleena,

    You last posted about using the ODS, are you still using this board? If so, then please ensure you are using the correct binary: xwr64xxODS_mmw_demo.bin.  The DSP version is not compatible.

    If the above does not work: It seems that you are using a single TX, is this desired? Typically multiple TXs are used. Furthermore, could you please post the entire config as printed in the console? Please also post a screenshot of the "setup details" and "scene selection" that you have selected.