Part Number: AWR1443
I have read several TI training documents, and find that the angle resolution is determined by the number of receiving antenna.
The formula is : angle resolution = 2 / N, and the doa algorithm is based on angle-FFT.
However, there's some subspace algorithms, such as , MUSIC ,ESPRIT, and they were called super-resolution algorithms.
Does this mean these super-resolution algorithms can increase the angle resolution.
For example, if there is only 1 TX and 4 RX , in the angle-FFT, the resolution is 28.5deg.
While I choose MUSIC algorithm , will the angle resolution increase? What is the formula?