We design and develop a 100KHz drive flyback converter power supply with 100V AC 50/60Hz input and 12V 6A output.
In order to configure the secondary-side synchronous rectification, the circuit was configured according to the application circuit example of UCC24612 using UCC24612. However, the FET drive signal of synchronous rectification is terminated in an instant, and synchronous rectification does not operate according to the specifications. Removing noise from the rectifier voltage signal with a CR filter improves the situation slightly, but the FET gate drive signal is only emitted for a short period of time.
The rectifier circuit on the negative side is configured, but it does not operate according to the specifications.
I am designing in Japan, is it possible to get support?