Hi,
Is output Hi-Z with below setting?
IN: L
NO: Hi-Z
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hey David,
As Clemens mentioned, the IN pin controls the state of the connection between NO, determining whether it is connected or disconnected.
From section 7.4 in the datasheet you can see the truth table of how this device functions given the IN input.
When IN is L, the NO to COM path is HI-Z.
Thanks,
Rami