Other Parts Discussed in Thread: OPA991, TMUX8108, TMUX7308F
We are using two TMUX7208 as the cell selector mux in conjunction with an OPA991 for measurement of cell voltages in a battery-string. We use the single supply mode of the TMUX and have it hooked up to the top cell-voltage (+33.6V) and ground (0V). The OPA uses the same supply.
Due to the rather high quescent current of all three devices, we want to be able to shut them down along with the MCU power domain on the battery pack.
We have looked at two solutions.
A) A high side switch: This removes +33 V from the TMUX VIN. But according to the datasheet, S1-S8 must not exceed VIN+0.5V. There is nowhere i can figure out how the protection input works. So i have actually fitted diodes from each S1-S8 to VIN to ensure this is never exceeded. Therefore the high-side switch will only work, if the S1-S8 can be allowed to exceed VIN when the device is not powered. (And i remove the diodes)
B) A low side switch. Cutting the GND off using a low side FET. This has the simple advantage that we can use a singe low-side TTL level N-FET easy to operate from the MCU. Hoever again this is questionable, if it's allowed.
I hope you can help us with some technical knowledge on how to disable these devices.