Hello Team,
The datasheet specified that V.ih and V.il are 1 V and 0.4 V. Is this for any supply voltage?
We need to ensure that the IN[1:4] pins can be controlled by 1.8 V when supplied by Vcc of 3.3 V
Thanks,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Team,
The datasheet specified that V.ih and V.il are 1 V and 0.4 V. Is this for any supply voltage?
We need to ensure that the IN[1:4] pins can be controlled by 1.8 V when supplied by Vcc of 3.3 V
Thanks,
Hi Alice,
For a supply voltage of 3.3V, the VIH = 1.4V and the VIL = 0.5V. This can be seen in table 6.6 of the datasheet under the Digital Control Inputs (IN1 - IN4) section.
The TS3A4751 digital input is 1.8V compatible when using a 3V supply.
Thanks,
Tyler