This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi teams,
Good day!
My customer use the TS12A4514/TS12A4515 , and there is confusion about the IN pin logic voltage.
Regarding the "Electrical Characteristics for 12-V Supply " in datasheet, Vin for " Digital Control Input (IN) " pin should be 5V ~ V+.
But "Logic-Level Thresholds" on page 7 showed that "when V+ reaches 12 V, the level threshold is about 3 V".
Is there a mistake in our understanding? When V+ is 12v, what is the at least input voltage for high logic?
Datasheet: https://www.ti.com/lit/ds/symlink/ts12a4514.pdf?ts=1656659260715&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct%252FTS12A4514
Best Regards
Miao Bai
Hi Miao,
The "Electrical Characteristics for 12V supply" table is correct, the logic threshold for VIH is 5V when V+ is 12V. The "Logic-Level Thresholds" on page 7 is saying that when V+ is at 12V, the threshold is now roughly 3V above the TTL (Transistor-Transistor Logic) interface standard logic threshold of 2.8V since it is now 5V. The datasheet is attempting to highlight a concern that designers should keep in mind if they use the TS12A4514/15 in a system designed around TTL interface. It is not conflicting with the "Electrical Characteristics for 12V supply" table.
Thanks,
Tyler