This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello, all
Now we are looking for some replaceable solution from LTC2859 for our new model.
I think SN65HVD23 plus some bus switch solution, which is like MAX14759 or MAX14763, would be needed to realize this. (Sorry, but I just could find suit solution for MAXIM part, but would like to find on TI's one instead.)
Please let us know which TI's bus switch part would be suit for this case.
Thank you for your information.
Best regards,
Hello Atsushi,
I'm moving this post to the switches forum so the team there can answer your question. I looked at the catalog myself and it seems that the TS12A4514 or TS12A4515 might be what you are looking for, but I'm not sure if those are the best options.
Team, can you tell us what part would be good for switching on and off a termination resistor?
Thanks,
Jason Blackman
Hello Atsushi,
Could you please provide more details on the exact requirements for the switch? Details such as:
Regards,
Andrew
Hello, thank you for your prompt reply.
With regard to your inquiries, please see the comment below;
VCC range
=>3.0~5.5V, which is same as MAX14759.
Analog signal range (referenced to Ground)
=>-25~25V, which is same as MAX14759.
Now I am collecting the information for another requirements internally, then would like to feedback to you later.
Thank you in advance for your consideration.
Best regards,
Hello, thank you for your support.
With regard to your inquiries, please see my comment as below;
Max data rate for signal being passed through switch(or frequency)
=>The data rate is less than 200kbps.
Ron requirements
=>1ohm(max), which is same as MAX14759.
Con/Coff requirements
=>Not specified, since this term is not defined on MAX14759.
Leakage current requirements
=>+/-200nA(max), which is same as MAX14759.
VCC range
=>3.0~5.5V, which is same as MAX14759.
Analog signal range (referenced to Ground)
=>-25~25V, which is same as MAX14759.
Please feedback us with your comment whether you could recommend any TI's part could be replaced in accordance with these terms.
Thank you in advance for your information.
Best regards,
Hello Atsushi,
I apologize for the delay here but after speaking with other teams in TI we do not have a switch that meet the application needs.
Regards,
Andrew