Other Parts Discussed in Thread: SN74CB3T3245, SN74CB3Q3245
Dear Specialists,
My customer is considering SN74CB3345 instead of SN74CB3245.
They have a question about OE pin.
I would be grateful if you could advise.
---question
We are considering SN74CB3Q3345 as a replacement for SN74CB3T3245.
The SN74CB3T3245 and SN74CB3Q3345 differ in the function of pin1.
Current: SN74CB3T3245DGVR 1pin function: NC
Substitute: SN74CB3Q3345DGVR 1pin Function: OE
When the SN74CB3Q3345DGVR pin 19: OE~ pin is connected to GND, is it possible to use pin 1: OE pin left open?
In addition, 1pin: Is OE terminal internally pulled up or pulled down?
Bus Switch is fixed to ON state.
---
I appreciate your great help in advance.
Best regards,
Shinichi